AXIS#.IL.AINSCALE

Description

AXIS#.ILClosed"Instruction list" This is a low-level language and resembles assembly.AINSCALE sets the analog current scale factor that scales the analog input (AINx.VALUE) for AXIS#.OPMODE = 0 (analog torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode).

This parameter is the motor current that will be commanded for every 1V on the analog input. This value may be higher or lower than the current limits, but the commanded current will be limited by the application current limit (AXIS#.IL.LIMITN and AXIS#.IL.LIMITP ).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A/V

Range

-22.4 to 22.4 A/V

Default Value

0 A/V

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Related Topics

Analog Input

Block Diagram for TorqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Loop